SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
The voltage reference mode must be configured by using either the ADC_setVREF() or the SetVREF() functions, depending on the header files used, provided in the C2000Ware Device SDK. Using either of these functions makes sure that the correct trim is loaded in the ADC trim registers. This function must be called at least once after a device reset. Do not configure the voltage reference mode by directly writing to the ANAREFCTL register.