SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
Each MCPWM module is connected to eight TZn signals (TZ1 to TZ8). All eight TZn signals are sourced from the PWM X-BAR that is inherited from a type-4 ePWM. Refer to the Crossbar (X-BAR) chapter to see what signals can be routed to the MCPWM module to be used as a trip source. These signals indicate external fault or trip conditions, and the MCPWM outputs can be programmed to respond accordingly when faults occur.
Figure 15-32 illustrates the trip-zone submodule within the MCPWM.
Figure 15-32 Trip-Zone
Submodule