SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
This sections gives details about the entry point addresses for various boot modes. These entry points direct the boot ROM what address to branch to at the end of booting as per the selected boot mode.
Table 4-16 gives details about the entry point addresses for Flash boot mode.
Table 4-17 gives details about the entry point addresses for RAM boot mode.
Table 4-18 gives details about the entry point addresses for Secure Flash boot mode.
| Option | BOOTDEFx Value | Flash Entry Address | Flash Sector | Package Supported |
|---|---|---|---|---|
| 0 (default) | 0x03 | 0x0008 0000 | CPU1 Bank 0 Sector 0 | All |
| 1 | 0x23 | 0x0008 8000 | CPU1 Bank 0 Sector 32 | All |
| Option | BOOTDEFx Value | RAM Entry Point (Address) | Package Supported |
|---|---|---|---|
| 0 | 0x05 | 0x0000 0000 | All |
| Option | BOOTDEFx Value | Flash Entry Address | Flash Sector | Package Supported |
|---|---|---|---|---|
| 0 (default) | 0x0A | 0x0008 0000 | CPU1 Bank 0 Sector 0 | All |
| 1 | 0x2A | 0x0008 8000 | CPU1 Bank 0 Sector 32 | All |