SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Target transmitter mode can be entered only from target receiver mode. With any of the address formats (a), (b), or (c) (see Figure 12-11), the target transmitter is entered if the target address byte is the same as its own address and bit R/W_ is transmitted, if R/W_ is high. The target transmitter shifts the serial data out on the data line SDA in sync with the clock pulses that are generated by the controller device. It does not generate the clock but it can hold clock line SCL low while intervention of the LH is required (XUDF).