SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Figure 12-11 shows the I2C data transfer formats in F/S mode.
The first word after an S condition consists of 8 bits. In acknowledge mode, an extra dedicated acknowledgment bit is inserted after each byte.
In addressing formats with 7-bit addresses, the first byte is composed of 7 MSB target address bits and 1 least-significant bit (LSB) R/W_ bit.
The LSB R/W_ bit of the address byte indicates the transmission direction of the data bytes that follow it. If R/W_ is 0, the controller writes data to the selected target; if it is 1, the controller reads data from the target.
In addressing formats with 10-bit addresses, the structure of the first byte is 11110XXY, where XX is the two MSBs of the 10-bit addresses, and Y is the R/W_ bit. If the R/W_ bit is 0, the next byte contains the last 8 bits of the target address. If the R/W_ bit is 1, the next byte contains data transmitted from the target to the controller.