SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The selection of the Pixel clock rate and DPHY Bit clock rate should ideally match based on the ratio of bpp on the pixel side compared to the tx_byte_clk. The timing for the horizontal sync, back and front porch will also be configured to allow the pixel data to be transferred without any over or underflow of the DPI FIFO.
The DPI FIFO fill level register (DPI_CFG) can be used to track that the parameters are sufficient and that any clock variation can still be handled by the FIFO depth. This register will show the pixel data held in the buffer, so during the HSA and HBP packet generation stages DPI pixel data will be stored and this value will increment. Once the data packet is being generated, the DPI_CFG level will remain constant, as the buffer is emptied at the same bandwidth as it is filled. Finally, the value will reduce to zero during the HFP stage.
The packet length of the HFP can be adjusted to help absorb small differences in the pixel_clk to tx_byte_clk relationship. The DSITX controller will concatenate all of the packets during High Speed transmission, so for example adding to the byte value of the HFP will make the bytes at the end of the packet move to align on another lane.
The packets that follow will then be concatenated and aligned to the next available lane, so if the tx_byte_clk is faster than the expected pixel clock times bpp the extra byte will delay the start of the new line tx_byte_clk × extra_byte/lanes.
Figure 12-553, Video coherency, illustrates the impact of increasing the HFP by one byte so that the next line begins ¼ tx_byte clock later. This allows averaging out across the line length of small differences in the pixel to tx_byte clocks when the tx_byte clock is not ideally matched to the expected pixel clock multiplied by bpp.
The DPI_CFG register will show any clock misalignment as an increasing/decreasing value for the FIFO fill level on each line of pixels (must be read mid-line for an accurate reading of the level). When the byte count adjustment is made, the DPI_CFG register will return to the original fill level value every four lines.