SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
RAT block is responsible to do a region based address translation. For each region, user can define the starting address and size of the region and remapping the transactions to use a new address range.
The starting address and region size need to be aligned. For example, if the region size is 16KB, the starting address for that region needs to be 16KB aligned. And region size should be minimum 4KB or larger to avoid transactions cross the region boundaries.
Each RAT block supports multiple programmable regions. And it is important that those regions are not overlapping with each other.
RAT block is by default disabled, which means RAT block does not do address remapping. The 32b address coming from R5 core is directly sent out to the SoC level. The user can program each RAT remapping region individually. For the transactions does not hit any remapping region, RAT block just simply forwards the transactions to the SoC level with its original address.