SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The PCIe subsystem supports bypassing the outbound address translation in the PCIe controller when the casel value on the VBUSM target interface is non-zero.
The device DMA has the ability to send transactions to alternate address maps which are external to the local device. This is achieved by using casel identifier in the DMA descriptors. There are three requirements that need to be met in the PCIe subsystem when using this mode in the DMA, namely:
To meet these requirements, the PCIe subsystem uses the cvirtid values on the VBUSM target interface to filter transactions based on initiator credentials. The VMAP block in the PCIe subsystem has a virtid match register (PCIE_VMAP_OB_VIRTID_MATCH) and a set of 32 registers that can be used to program the descriptor fields when the ATU logic in the PCIe controller is bypassed.
The PCIe subsystem will filter outbound VBUSM target transactions that have a non-zero casel value. If the cvirtid[11:5] attribute of the VBUSM target transaction matches the value programmed in the PCIE_VMAP_OB_VIRTID_MATCH register, the credentials of the transaction initiator are verified. The cvirtid[11:5] value should also be non-zero for a successful match.
When the credentials match, the ATU of the PCIe controller is bypassed . The cvirtid[4:0] is used to select one of the 32 PCIE_VMAP_DESC_j descriptor registers. These registers can be programmed to assign the BDF and TC values to the outbound PCIe transaction. If the PCIE_VMAP_DESC_j[16] BD_EN0 register bit is set, then the bus, device and function numbers are all set from the external descriptor registers. If the BD_EN bit is not set, then the bus and device numbers are assigned by the PCIe controller using the values captured during enumeration. If ARI mode is enabled (in the PCIE_CORE_PFn_I_SRIOV_CTRL_STATUS_REG register), the function number uses the PCIE_VMAP_DESC_j[7:0] DEV_FUNC_NUM register field. If ARI mode is not enabled, the device number uses PCIE_VMAP_DESC_j[7:4] DEV_FUNC_NUM field and the function number uses the [3:0] DEV_FUNC_NUM field. The ARI mode is a PCIe controller hardware configuration option that is enabled for PCIe endpoints that support SR-IOV.
If the credentials of the initiator fail to match the programmed value in the PCIE_VMAP_OB_VIRTID_MATCH register, the VBUSM target transaction is then flushed by the bridge and is not submitted to the PCIe controller. The VBUSM2AXI2 bridge will return a protection error status for both read and write transactions. In addition, the write data is discarded and the correct number of read data phases with data value of zero are returned.