SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The A53SS does not have an integrated watchdog timer. Instead, this feature is provided externally by the Real Time Interrupt Module (RTI) module, which implements a windowed watchdog timer capable of issuing warm reset to the SoC, when necessary.
For more details on the RTI windowed watchdog feature, see Real Time Interrupt Module (RTI/WWDT).