SPRUJB6B November 2024 – May 2025 AM2612
When the UART_LSR_UART register is read, the UART_LSR_UART[4:2] bit field reflects the error bits (BI: break condition, FE: framing error, PE: parity error) of the character at the top of the RX FIFO (the next character to be read). Therefore, reading the UART_LSR_UART register and then reading the UART_RHR register identifies errors in a character.
Reading the UART_RHR register updates the BI, FE, and PE bits (see Table 13-75 for the UART mode interrupts).
The UART_LSR_UART[7] RX_FIFO_STS bit is set when there is an error in the RX FIFO and is cleared only when no errors remain in the RX FIFO.
Reading the UART_LSR_UART register does not cause an increment of the RX FIFO read pointer. The RX FIFO read pointer is incremented by reading the UART_RHR register.
Reading the UART_LSR_UART register clears the OE bit if it is set (see Table 13-75 for the UART mode interrupts).