SPRUJB6B November 2024 – May 2025 AM2612
The R5FSS has seven reset inputs:
The above resets can be controlled through RCM registers.
In addition to the reset signals, there are two halt signals:
These halt signals keep the CPUs from fetching instructions when they come out of reset. The main use is to have the CPUs halted until the TCMs are loaded (when booting from TCM), though halt could be used for any other purpose. See R5 Core Halting and Unhalting for more details.