SPRUJB6B November 2024 – May 2025 AM2612
In systems, the modulator clock can be generated using PWMs. Assuming all the SD-CLKs see the same delay on board traces, you can potentially use just one clock to clock multiple filters; thereby, saving on the number of pins used for SDFM. To enable this, Filter1 SDCLK (SDFM-CLK0) can possibly apply to other filter channels if required. The SDCTLPARAMx.SDCLKSEL register bit field can be configured to select filter channel SDCLK. It is also possible to drive SD0 FILTER0 clock from the pinmux to SD1 FILTER0 by configuring CONTROLSS_CTRL.SDFM1_CLK0_SEL. See Figure 7-367 to view this feature.