SPRUJB6B November 2024 – May 2025 AM2612
When monitoring the PWMs, PWMs can be tripped by the external trip event that is forced to a known state. Under this condition, PWM signal monitoring is disabled temporarily until the trip condition is cleared. To support this feature, PWM trip signals are brought into eCAP module through external XBARs. In addition, an internal MUX is provided to select one of many XBAR signals. Signal monitoring is disabled as long on selected trip signal is active. Note that signal monitoring is automatically enabled when trip condition is cleared.
Figure 7-313 ECAP Signal Monitoring Unit Trip Signals