SPRUJB6B November 2024 – May 2025 AM2612
Two clocks are provided to the MCAN module:
Within the MCAN module there is a synchronization mechanism implemented to ensure safe data transfer between the two clock domains. There is synchronization between the signals from the Host clock domain to the CAN clock domain and vice versa and between the reset signal to the Host clock domain and to the CAN clock domain.
ICLK must always be higher or equal to FCLK, in order to achieve a stable functionality of the MCAN module. Here, also the frequency shift of the modulated ICLK has to be considered:
f0,ICLK ± ΔfFM,ICLK ≥ fFCLK
For more information on how to configure the relevant clock source registers, see Section 6.4, Clocking and the device-specific Data sheet.