SPRUJB6B November 2024 – May 2025 AM2612
This section describes common instructions for FIR and MIR mode programming.
At the end of a frame reception, the CPU reads the line status register (UART_LSR_UART) to detect errors in the received frame.
When the UART_MDR1[6] SIP_MODE bit is set to 1, the TX state-machine always sends one SIP at the end of a transmission frame. However, when the SIP_MODE bit is set to 0, SIP transmission depends on the UART_ACREG[3] SEND_SIP bit.
The CPU can set the SEND_SIP bit at least once every 500 ms. The advantage of this approach over the default approach is that the TX state-machine does not have to send the SIP at the end of each frame, thus reducing the overhead required.