SPRUJB6B November 2024 – May 2025 AM2612
The frame watchdog is an additional feature the receiver can use to monitor for any error conditions. This dedicated watchdog monitors the duration for a single frame to be received. The watchdog starts incrementing at the time the receiver detects a proper start of frame condition. If the end of frame condition is not detected within the expected number of SYSCLK cycles, the frame watchdog is triggered that can generate an interrupt or be monitored by software.
This watchdog is automatically started and stopped at the start-of-frame and end-of-frame conditions, respectively. The frame watchdog is connected to SYSCLK.
To configure the frame watchdog for operation:
The frame watchdog is now enabled and can detect a failed frame.
If the RX_FRAME_WD_CNT reaches the value programmed in RX_FRAME_WD_REF, the RX_EVT_STS_ALT1_.FRAME_WD_TO flag is set. If enabled, an interrupt can be generated on this event.
If the frame watchdog interrupt ever occurs, the receiver core is in an invalid state to receive a new transmission. The only way to recover from a frame watchdog time out is to undergo a soft reset, and subsequently resynchronizing with the transmitter.