SPRUJB6B November 2024 – May 2025 AM2612
INFRA1 VBUSP interconnect connects with the PERI VBUSP interconnect through a single target port catering to all initiators on the PERI VBUSP. Accessing a particular target by multiple initiators at the same time will be arbitrated in this interconnect. The diagram below shows the peripherals which are target ports for the INFRA1 VBUSP interconnect.
There is no access restriction since its a single initiator, multiple target interconnect.