SPRUJB6B November 2024 – May 2025 AM2612
Any external memory or ASIC device attached to the GPMC external interface can be accessed by any device system host within the GPMC 128MB address space. For more information, see Memory Map.
Even though GPMC supports total address space of 1GB, only 128MB are physically available in this device.
The GPMC 128MB address space can be divided into a maximum of four chip-select regions with programmable base address and programmable chip-select size. The chip-select size is programmable from 16MB to 256MB (must be a power-of-two) and is defined by the mask field. Attached memory smaller than the programmed chip-select region size is accessed through the entire chip-select region (aliasing).
Each chip-select has a 6-bit base address encoding and 4-bit decoding mask, which must be programmed according to the following rules:
Figure 13-126 Chip-Select Address Mapping and Decoding MaskFor example, to map the 128MB address space (from ), the GPMC_CONFIG7_i[5-0] BASEADDRESS bit field should be set to 28h.
Eg : 68000000h = 0110_1000_0000_0000_0000_0000_0000_0000b
Base Address[29:24] = 10_1000 = 28h
Chip-select configuration (base and mask address or any protocol and timing settings) must be performed while the associated chip-select is disabled through the GPMC_CONFIG7_i[6] CSVALID bit (where i stands for the GPMC chip-select i, where i = 0 to 3). In addition, a chip-select configuration can be disabled only if there is no ongoing access to that chip-select. This requires monitoring the activity of the prefetch or write-posting engine if the engine is active on the chip-select. Also, the write buffer state must be monitored to wait for any posted write completion to the chip-select.
Any access attempted to a nonvalid GPMC address region (CSVALID disabled or address decoding outside a valid chip-select region) is not propagated to the external interface and a GPMC access error is posted. In case of overlapping chip-selects, an error is generated and no access occurs on either chip-select.
CS0 is the only chip-select region enabled after a power up or GPMC reset.
Although the GPMC interface can drive up to four chip-selects, the frequency specified for this interface is for a specific load. If this load is exceeded, the maximum frequency cannot be reached. One solution is to implement a board with buffers to allow the slowest device to maintain the total load on the lines at the value specified in the device-specific Datasheet.