SPRUJB6B November 2024 – May 2025 AM2612
Flags in the MMC/SD/SDIO host controller show status of communication with the card:
Error conditions generate interrupts. See Table 13-250 and register description for more details.
| Error hold in the MMC_STAT Register | CC | TC | Comments | |
|---|---|---|---|---|
| 29 | BADA | No dependency with CC or TC. BADA is related to the register accesses. Its assertion is not dependent of the ongoing transfer. | ||
| 28 | CERR | 1 | CC is set upon CERR. | |
| 22 | DEB | 1 | TC is set upon DEB. | |
| 21 | DCRC | 1 | TC is set upon DCRC. | |
| 20 | DTO | DTO and TC are mutually exclusive. DCRC and DEB cannot occur with DTO. | ||
| 19 | CIE | 1 | CC is set upon CIE. | |
| 18 | CEB | 1 | CC is set upon CEB. | |
| 17 | CCRC | 1 | CC can be set upon CCRC - See CTO comment | |
| 16 | CTO | CTO and CC are mutually exclusive. CIE, CEB and CERR cannot occur with CTO. CTO can occur at the same time as CCRC it indicates a command abort due to a contention on CMD line. In this case no CC appears. | ||
MMC_STAT[21] DCRC event can be asserted in the following conditions: