SPRUJB6B November 2024 – May 2025 AM2612
The PLL can be coupled with an HSDIVIDER module to generate additional clocks which are divided down from the PLL lock frequency.
The HSDIVIDER has two input clocks:
The HSDIVIDER provides 4 post divider clocks whose frequency is given by:
Where:
CLKINPHIFLDO is the input clock frequency.
The clocking subsytem provides registers to directly configure the final divide value of "DIVx+1". When specifying the desired HSDIV value to use, it should be specified as "DIVx-1".
The "DIVx+1" reset value is 4.