If the clock to the CMPSS module is disabled while the comparator is active, the following behavior can be expected:
- The comparator remains unaffected and continues to trip from voltages on the inputs.
- If the reference 12-bit DAC is driving the negative input of the comparator, the voltage on the negative input remains static and unaffected but DACVALA can no longer be updated from the ramp generator or DACVALS.
- The ramp generator, synchronize block and digital filter freeze on their current states.
Enabling the clock to the CMPSS restores the clock to the state before the clock was disabled.