SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
Trip signal is generated upon signal monitoring errors. All the signal monitoring error events are OR-ed and provided as a trip output. The trip signal remains active until interrupt flags are cleared in ECFLG register. Trip cannot be disabled in eCAP, instead the trip has to be deselected in external XBAR if there is no intent to use the feature.
The ECAPx.TRIPOUT signal can be used to trip the EPWM modules. This can cause the EPWMx.TRIPOUT signal, which is fed back to eCAP module to also trip, which can disable the monitoring function and also cause a false trip if this feature is enabled. Therefore, if ECAPx.TRIPOUT is used, it is recommended that EPWMx.TRIPOUT be disabled.