SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
TMU operations can take 8 to 10 Effective R5 CPU cycles to return the result after OP1 is written to trigger an operation. There are 8 result registers in the TMU accelerator. The result is written to one of the result registers when the operation completes. The TMU accelerator contains multiple result registers to serve as temporary storage to enable back to back operations in consecutive cycles and keep the results separate.
Listed below are the supported operations and number of result registers needed per operation: