When the receiver FIFO is enabled in the FIFO
control register (FCR), mapped in the MSB part of the register UART_INT_FIFO, and
the receiver interrupts are enabled in the interrupt enable register UART_INT_EN,
the interrupt mode is selected for the receiver FIFO. The following are important
points about the receiver interrupts:
- The receiver data-ready interrupt is issued to the CPU when the FIFO has reached the trigger level that is programmed in FCR. It is cleared when the CPU or the DMA controller reads enough characters from the FIFO such that the FIFO drops below its programmed trigger level.
- The receiver line status interrupt is generated in response to an overrun error, a parity error, a framing error, or a break. This interrupt has higher priority than the receiver data-ready interrupt. For details, see Section 7.3.8.3.4.
- The data-ready ([0]DR) bit in the line status
register - UART_LSR1, indicates the presence or absence of characters in the
receiver FIFO. The [0]DR bit is set when a character is transferred from the
receiver shift register (RSR) to the empty receiver FIFO. The [0]DR bit remains
set until the FIFO is empty again.
- A receiver time-out interrupt occurs if all of the following conditions exist:
- At least one character is in the FIFO,
- The most recent character was received more than
four continuous character times ago. A character time is the time
allotted for 1 START bit, n data bits, 1 PARITY bit, and 1 STOP
bit, where n depends on the word length selected with the WLS0
and WLS1 bits of the line control register UART_LCTR. See Table 7-73.
- The most recent read of the FIFO has occurred more than four continuous character times before.
- Character times are calculated by using the baud rate.
- When a receiver time-out interrupt has occurred, it is cleared and the time-out timer is cleared when the CPU or the EDMA controller reads one character from the receiver FIFO. The interrupt is also cleared if a new character is received in the FIFO or if the URRST bit is cleared in the power and emulation management register - PWM.
- If a receiver time-out interrupt has not occurred, the time-out timer is cleared after a new character is received or after the CPU or EDMA reads the receiver FIFO.
When the transmitter FIFO is enabled in
UART_INT_FIFO[0] IIR_IPEND bit and the transmitter holding register empty (THRE)
interrupt is enabled in UART_INT_EN[1] ETBEI bit, the interrupt mode is selected for
the transmitter FIFO. The THRE interrupt occurs when the transmitter FIFO is empty.
It is cleared when the transmitter hold register (THR) UART_RBR_TBR[7-0] RBR_DATA
bitfield is loaded (1 to 16 characters may be written to the transmitter FIFO while
servicing this interrupt) or the [3-1]IIR_INTID bitfield is read in the interrupt
identification register UART_INT_FIFO.
Table 7-73 Character Time for Word Lengths| Word Length (n) | Character Time | Four Character Times |
|---|
| 5 | Time for 8 bits | Time for 32 bits |
| 6 | Time for 9 bits | Time for 36 bits |
| 7 | Time for 10 bits | Time for 40 bits |
| 8 | Time for 11 bits | Time for 44 bits |