SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The PRU-ICSS UART0 peripheral can be placed in reduced-power modes to conserve power during periods of low activity. The power management of the PRU-ICSS UART0 peripheral and other PRU-ICSS peripherals is controlled by the device Reset Control Manager (RCM). The RCM acts as a power management controller for all of the peripherals on the device. For more details on the power management procedures using the PSC, refer to the Power Management section.