SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The PRU core directly drives the MII transmit interface via its R30 internal register. The contents of R30 register and RX Data from receive interface are taken and fed into a transmit FIFO (TX L2 FIFO - 64 Bytes).
Data to be transmitted is loaded into the TX L1 FIFO. The transmit FIFO (TX L1) stores up to 40 Bytes of transmit data. Note that this includes the preamble bytes. From the transmit FIFO (TX L1), the data is sent to the MII TX port of the PHY by the MII_RT transmit logic.
The transmit FIFO also has the capability to be reset through software (TX_RESET). When reset, all contents of transmit FIFO are purged and this may result in a frame not getting transmitted as expected, if the transmission is already ongoing. Any new data written in the transmit FIFO results in a new frame being composed and transmitted. An overflow event will require a TX_RESET to recover from this condition.
There are four dependencies that must be true for TX_EN to assert:
The transmit interface also provides an underflow error signal in case there was no data loaded when TX_EN triggered. The transmit underflow signal is mapped to the INTC in PRU-ICSS. The current FIFO fill level cannot be accessed by PRU firmware. The firmware can issue an R31 command via R31 bit 29 (TX_EOF) to indicate that the last byte has been written into the TX FIFO.