SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
| Bit | Field Name | Description |
|---|---|---|
| 7 | ERROR_CRC | ERROR_CRC indicates that the frame has a CRC mismatch. This bit is valid when the RX_EOF bit is set. It should be noted that ERROR_CRC bit is ready in early status, which means it is calculated before data is available in RX L1 FIFO. ERROR_CRC will only be set for one entry, self clear on next entry. |
| 6 | ERROR_NIBBLE | ERROR_NIBBLE indicates that the frame ended in odd nibble. It should be considered valid only when the RX_EOF bit and pr1_mii0/1_rxdv are set. Nibble counter is enabled post SFD event. It should be noted that ERROR_NIBBLE bit is ready in early status, which means it is calculated before data is available in RX L1 FIFO. ERROR_NIBBLE will only be set for one entry, self clear on next entry. |
| 5 | RX_SOF | RX_SOF transitions from low to high when the frame data starts to arrive and pr1_mii0/1_rxdv is asserted. Note: There will be a small sync delay of 0ns – 5ns. It should be noted that RX_SOF bit is ready in early status, which means it is calculated before data is available in RX L1 FIFO. RX_SOF will only be set for one entry, self clear on next entry. |
| 4 | RX_SFD | RX_SFD transitions from low to high when the SFD sequence (0xD5) post RX_SOF is observed on the receive MII data. It should be noted that RX_SFD bit is ready in early status, which means it is calculated before data is available in RX + L1 FIFO. RX_SOF will only be set for one entry, self clear on next entry. |
| 3 | RX_EOF | RX_EOF indicates that the frame has ended and pr1_mii0/1_rxdv is de-asserted. It also validates the CRC match bit. Note: There will be a small sync delay of 0ns – 5ns. It should be noted that RX_EOF bit is ready in early status, which means it is calculated before data is available in RXL1 FIFO. If RX_L2_EOF_SCLR_DIS = 1, then RX_EOF will remain set until RX_EOF_CLR event. Otherwise, RX_ERROR is self-clearing on next entry. |
| 2 | RX_ERROR | RX_ERROR indicates one or more of the following errors occurred:
|
| 1 | STATUS_RDY | STATUS_RDY is set when RX_EOF or write pointer advanced by 2. This is a simple method for software to determine if RX_EOF event has occurred or new data is available. If RX_EOF is not set, all status bits are static. |
| 0 | RX_ERR | RX_ERR is set to 1 when pr1_mii0/1_rxer is asserted while pr1_mii0/1_rxdv bit is set. It will get set for first pr1_mii0/1_rxer event and self clear on SOF for the next FRAME. |