SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The pseudo code:
Read Controller: This is optimized from a 2D-transfer to a 1D-transfer such that the read side is equivalent to EDMA_TPTCn_PCNT[15:0] ACNT = 64, EDMA_TPTCn_PCNT[31:16] BCNT = 1.
Cmd0 = 64 byte
Write Controller: Because DBIDX != ACNT, it is not optimized.
Cmd0 = 8 byte, Cmd1 = 8 byte, Cmd2 = 8 byte, Cmd3 = 8 byte, Cmd4 = 8 byte, Cmd5 = 8 byte, Cmd6 = 8 byte, Cmd7 = 8 byte.
Read Controller: Read address is not aligned.
Cmd0 = 1 byte, (now the SADDR is aligned to 64 for the next command)
Cmd1 = 64 bytes
Cmd2 = 63 bytes
Write Controller: The write address is also not aligned.
Cmd0 = 63 bytes, (now the DADDR is aligned to 64 for the next command)
Cmd1 = 64 bytes
Cmd2 = 1 byte