SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
This section identifies the requirements of initializing the surrounding modules when the module has to be used for the first time after a device reset. This initialization of surrounding modules is based on the integration and environment of the MMC/SD/SDIO modules.
| Surrounding Modules | Comments |
|---|---|
| Power, Reset, and Clocking | Module interface and functional clocks must be enabled. For more information on power, reset, and clock management, see the corresponding sections within the Device Configuration chapter. |
| Control Module | Module-specific pad muxing and configuration must be set in the control module. For more information, see the section within the Device Configuration chapter. |
| (optional) VIM | VIM configuration must be done to enable the interrupts from the SD module. See Interrupts . |
| (optional) EDMA | DMA configuration must be done to enable the module DMA channel requests. See EDMA. |
| (optional) Interconnect | For more information about the interconnect configuration, see System Interconnect. |
The Vector Interrupt Manager and the EDMA configurations are necessary if the interrupt and DMA based communication modes are used.