SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The class of service mechanism can be enabled by setting to 0x1 the EMIF_READ_WRITE_EXECUTION_THRESHOLD[31] MFLAG_OVERRIDE bit. In this case EMIF services the order of commands given by the class of service rules described in the following paragraphs. If MFLAG_OVERRIDE is set to 0x0 then class of service does not apply. When MFLAG_OVERRIDE is 0x0 and the MFLAG is high then the EMIF alternates between one command coming from the MPU interface and one from the System interface and so forth. The MFLAG value is ignored if MFLAG_OVERRIDE is 0x1.
The commands in the Command FIFO can be mapped to two classes of service namely 1 and 2. The mapping of commands to a particular class of service can be done based on the priority or the master ID. The mapping based on priority can be done by setting the appropriate values in the EMIF_PRIORITY_TO_CLASS_OF_SERVICE_MAPPING register. The mapping based on master ID can be done by setting the appropriate values of master ID and the masks in the EMIF_CONNECTION_ID_TO_CLASS_OF_SERVICE_1_MAPPING and EMIF_CONNECTION_ID_TO_CLASS_OF_SERVICE_2_MAPPING registers. There are 3 master ID and mask values that can be set for each class of service. In conjunction with the masks, each class of service can have a maximum of 144 master IDs mapped to it. For example, a master ID value of 0xFF along with a mask value of 0x3 will map all master IDs from 0xF8 to 0xFF to that particular class of service.
Each class of service has an associated latency counter (EMIF_COS_CONFIG[23:16] COS_COUNT_1 and EMIF_COS_CONFIG[15:8] COS_COUNT_2). When the latency counter for a command expires, that is, reaches the value programmed for the class of service that the command belongs to, that command is executed next. If there is more than one command that has expired latency counter, the command with the highest priority is executed first. One exception to this rule is, if the EMIF_COS_CONFIG[7:0] PR_OLD_COUNT value expires for the oldest command in the queue. That command is executed first irrespective of priority or class of service. This is done to prevent the continuous blocking effect.
The EMIF_COS_CONFIG[7:0] PR_OLD_COUNT value is used to identify when the oldest command in the command FIFO has timed out. At this point during the arbitration process, this oldest command is issued regardless of the priority of the other commands in the FIFO. This feature is disabled when writing 0x0 to the EMIF_COS_CONFIG[7:0] PR_OLD_COUNT bit field. After issuing the oldest command, the other remaining commands in the FIFO are reordered by age. The next oldest command in the FIFO is given highest priority again and issued after the EMIF_COS_CONFIG[7:0] PR_OLD_COUNT value expires. If a new value in the PR_OLD_COUNT bit field is written during counting, that is, before PR_OLD_COUNT expires, the counter keeps working but if this value is smaller the oldest command is issued sooner and if this value is larger the oldest command is issued later.
The master ID mapping allows the same master ID to be put in both class of service 1 and 2. Also, a transaction might belong to one class of service if viewed by master ID and might belong to another class of service if viewed by priority. In these cases, the command will belong to both class of service. The EMIF will try executing the command as soon as possible, when the smaller of the two counters (EMIF_COS_CONFIG[23:16] COS_COUNT_1 and EMIF_COS_CONFIG[15:8] COS_COUNT_2) expires.