SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Packets transmitted or received on each Ethernet port can generate Ethernet Transmit Events or Ethernet Receive Events, respectively. The CPTS hardware will decode each packet to determine if it is a valid CPTS time sync event.
According to the IEEE 802.3 Ethernet standard, each Ethernet frame contains a 2-octet EtherType field to indicate which protocol is encapsulated in the PayLoad field, as shown in Figure 24-209. For standard time sync packets, this will contain the EtherType for the Precision Time Protocol (IEEE 1588), which is defined as 0x88F7. The CPTS hardware will compare this field to the TS_LTYPE1 field or the TS_LTYPE2 field (depending on which enable bit was set) in the CPSW_TS_LTYPE register, which should also be programmed to 88F7h.
When a virtual LAN is used, an additional 4-octet 802.1Q tag is inserted in the Ethernet frame before the EtherType field, as shown in Figure 24-209. To indicate to the CPTS hardware that a virtual LAN is in use, the Pn_TS_VLAN_LTYPE1_EN (or Pn_TS_VLAN_LTYPE2_EN) enable bit must be set in the Pn_CONTROL register. The EtherType for the 802.1Q tag is defined as 0x8100, and the CPTS hardware will compare this value to the VLAN_LTYPE1 (or VLAN_LTYPE2 depending on which enable bit was set) field in the CPSW_VLAN_LTYPE register, which should also be programmed to 0x8100.
When two stacked VLANs are used, two additional 4-octet 801.Q tags are inserted in the Ethernet frame before the EtherType field, as shown in Figure 24-209. In this case, both VLAN_LTYPE1 and VLAN_LTYPE2 must be enabled. The outer tag must match the value of the VLAN_LTYPE1 field, and the inner tag must match the value of the VLAN_LTYPE2 field.
Figure 24-209 Partial Ethernet-II Frames Showing Register Mapping of EtherTypes for a Simple Frame (1), a Single 1Q Tag Added (2), and Two 1Q Tags Added (3)To enable transmit/receive event packets on a given Ethernet port, perform the following steps, where n is the port number:
| Message Type | Value (hex) |
|---|---|
| Sync | 0 |
| Delay_Req | 1 |
| Pdelay_Req | 2 |
| Pdelay_Resp | 3 |
| Reserved | 4-7 |
| Follow_Up | 8 |
| Delay_Resp | 9 |
| Pdelay_Resp_Follow_Up | A |
| Announce | B |
| Signaling | C |
| Management | D |
| Reserved | E-F |
Once a transmitted or received packet is determined to be a valid time sync packet, the Ethernet Transmit Event or Ethernet Receive Event is loaded onto the Event FIFO. The CPTS_EVENT_HIGH register contains the Message Type and Sequence ID values from the original time sync packet. The CPTS_EVENT_LOW register contains the time stamp value when the packet arrived at the corresponding port.