SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The PAT engine can have up to 16 groups of initiators that share a set of four PAT views. The connection from an initiator to a PAT view is made through the DMM_PAT_VIEW register. Given that each PAT view index is coded on 4 bits, the DMM_PAT_VIEW register is a 64-bit register split into two 32-bit registers (DMM_PAT_VIEW0 for the first eight PAT view indexes and DMM_PAT_VIEW1 for the last eight PAT view indexes.
The PAT view index that corresponds to the initiator having the value i as the 4 most-significant bits (MSBs) of its L3 ConnID uses the view referenced in entry i of the DMM_PAT_VIEW. For example, the initiator 0xC7 uses the thirteenth view index of the DMM_PAT_VIEW register, the fifth view index in the DMM_PAT_VIEW1 register.
The PAT view index of the initiator i is found in the Vi field. The Wi field is aimed at writing the corresponding Vi. When writing to the DMM_PAT_VIEW registers, the only Vi view indexes that are updated are those having their corresponding Wi bit, and byte enable, set. The Wi bits are always read as 0. For instance, to set the PAT view indexes V3 and V7 to 2 and 1, respectively, the DMM_PAT_VIEW0 register must be written with 5000 6000h.