SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The OCM controller provides up to 12 programmable circular buffers that are mapped to virtual video frames to support sliced based on-the-fly video frame processing. Each circular buffer must be programmed with the following:
The circular buffer mode is enabled when the CFG_OCMC_CBUF_EN[0] CBUF_MODE_EN bit is set to 0x1. In addition, to enable certain circular buffer the corresponding bit in the CFG_OCMC_CBUF_EN[27:16] bit field must be set to 0x1. For example, to enable CBUF_0 both the CFG_OCMC_CBUF_EN[0] CBUF_MODE_EN and CFG_OCMC_CBUF_EN[16] CBUF_EN_0 bits must be set to 0x1.
The data transfers are made to the virtual frame addresses. The OCM controller translates these virtual addresses to SRAM addresses allocated for the CBUF. The address translation is done on-the-fly without leading to any additional latency and therefore has no performance impact on the overall operation of the OCM controller.
The L3_MAIN address range associated with the virtual frame addresses is the following:
When an initiator performs an access to these L3_MAIN addresses, these virtual frame addresses will be translated automatically by the OCM controller into SRAM addresses. Figure 15-109 shows the address mapping of the virtual frame addresses to CBUF addresses.
Figure 15-109 VBUF to CBUF Address MappingIt must be taken into account that the start address of a virtual frame always begins at the start of the CBUF. Since the virtual frame buffer size is not necessarily to be a multiple of the CBUF size, the last VBUF write location may not be the last line of the CBUF. As the CBUF read and write pointers are independently managed the initiators that are writing to and reading from the CBUF should be coordinated in order to avoid overflow and underflow conditions.