SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Different camera sources are interleaved on a line-by-line basis. The beginning of each line carries a Metadata tag that provides key information about that line. This Metadata tag is preceded by a SAV codeword in which F=0, V=0, and H=0.
At the end of the line, an EAV code is inserted with an appropriate number of padding pixels following it. This EAV code has F=0, V=0, and H=1. The startcodes used for the Metadata wrapped lines and the dummy lines form the Super Frame. The VIP_PARSER module has logic to parse out the super frame, analyze the Metadata tags, and frame buffer the line contents appropriately.