SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
MDIO_LINKINT is set if there is a change in the link state of the PHY corresponding to the address in the PHYADR_MON field of the MDIO_USERPHYSELn register and the corresponding LINKINT_ENABLE bit is set. The MDIO_LINKINT event is also captured in the MDIO_LINKINTMASKED register. When the GO bit in the MDIO_USERACCESSn register transitions from 1 to 0, indicating the completion of a user access, and the corresponding USERINTMASKSET bit in the MDIO_USERINTMASKSET register is set, the MDIO_USERINT signal is asserted. The MDIO_USERINT event is also captured in the MDIO_USERINTMASKED register.