SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
One Source Number for each Port can be cropped. Cropping is available for both Ancillary Data and Active Video.
For the Vertical Ancillary Data from Port A, cropping is enabled by setting the VIP_ANC_CROP_HORZ_PORT_A[15] ANC_BYPASS_N bit. The Source Number from Port A that gets cropped is defined by the VIP_ANC_CROP_HORZ_PORT_A[31:28] ANC_TARGET_SRCNUM register. VIP_ANC_CROP_HORZ_PORT_A[11:0] ANC_SKIP_NUMPIX, VIP_ANC_CROP_HORZ_PORT_A[27:16] ANC_USE_NUMPIX, VIP_ANC_CROP_VERT_PORT_A[11:0] ANC_SKIP_NUMLINES, and VIP_ANC_CROP_VERT_PORT_A[27:16] ANC_USE_NUMLINES define the region of the selected Source Number that is cropped and sent to DRAM. The Vertical Ancillary Data Cropping region is described in Figure 9-54.
Figure 9-54 Vertical Ancillary Data CroppingNote that for 8-bit input mode only, a setting exists that allow Vertical Ancillary data from both the Luma and Chroma channels to be captured. Both channels of Vertical Ancillary Data are captured when VIP_XTRA_PORT_A[14:13] ANC_CHAN_SEL_8B is set to “1x”. Thus, the number of data elements per line in this case is twice the equivalent number of Luma pixels per line. In other words, for this particular dual channel capture example, if there are 720 Luma pixels per line, then the total number of Vertical Ancillary Data Pixels in the source picture can be 2x720=1440 pixels.
For Active Video from Por tA, cropping is enabled by setting the VIP_CROP_HORZ_PORT_A[15] ACT_BYPASS_N bit. The Source Number from Port A that gets cropped is defined by the VIP_CROP_HORZ_PORT_A[31:28] ACT_TARGET_SRCNUM register.
VIP_CROP_HORZ_PORT_A[11:0] ACT_SKIP_NUMPIX, VIP_CROP_HORZ_PORT_A[27:16] ACT_USE_NUMPIX, VIP_CROP_VERT_PORT_A[11:0] ACT_SKIP_NUMLINES, and VIP_CROP_VERT_PORT_A[27:16] ACT_USE_NUMLINES define the region of the selected Source Number that is cropped and sent to DRAM. The Vertical Ancillary Data Cropping region is described in Figure 9-55
Figure 9-55 Active Video CroppingCropping for Port B works in a similar way to Port A. Since picture data is in 4:2:2 format, ANC_SKIP_NUMPIX( ACT_SKIP_NUMPIX) and ANC_USE_NUMPIX (ACT_USE_NUMPIX) must be evenly divisible by 2. If the output of VIP_PARSER is sent to a 4:2:2 to 4:2:0 converter, then ANC_USE_NUMLINES(ACT_USE_NUMLINES) must also be evenly divisible by 2.
Error cases in cropping occur when the crop window programmed is larger than the incoming video frame. Crop window errors normally result in the return of the crop region where the crop window overlays the incoming video frame. However, there is one problematic error cropping case, as illustrated in Figure 9-56.
The programmed crop window extends below the input picture and the last pixel of the input picture is not a part of the selected crop region. In this case, at the last pixel of the last line in the green crop output, there is no way to determine that this pixel is the last pixel of the cropped output.
Figure 9-56 Problematic Error Cropping CaseIn this case, the crop tool sends outs a single pixel with an endline and endframe when it reaches the last pixel of the input picture. If the green cropped region has n lines, the actual output from the crop tool will have n+1 lines and the width of the last line will be 1 pixel.
Figure 9-57 shows the endline (EL) and endframe (EF) signals corresponding to the last line of the cropped region. At the last line and last pixel of the cropped region, the crop tool will only output an endline. It cannot output an endframe at this point because the crop tool might get another line from the streaming input.
Later, on the same input line, the last pixel of the input frame appears. Here, the crop tool knows that the cropped region has ended. In this case, a single endline/endframe pixel is sent out to signal that the frame has ended.
There is no interrupt to notify that application level that a crop error has occurred.
Figure 9-57 Endline/Endframe Behavior for Error Cropping Case