SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
It is possible that an overflow can occur in the VIP_PARSER. Overflow detection is determined by reading the VIP_FIQ_STATUS register and checking for bits 8, 7, 5, 4, 3 and 2. If video is being captured, and any of these bits are set, it indicates that not all of the incoming video data was sent to DDR meory. VIP overflow can be caused by one of the following:
1. External pixel clock is faster than processing clock
2. DDR bandwidth is temporarily over-consumed
3. VIP scaler is being used inline with external video input, and is upscaling.
4. VIP scaler is being used inline with external video input, but has not been configured with scaler coefficients
5. VIP scaler is being used inline, but has not been enabled
6. External cables are connected or disconnected while the system is running, resulting in corrupted video streams going into the VIP
7. Bad external video cable, which causes corrupted video streams going into the VIP
Items 6 and 7 above are typically seen as noise events, where it is likely that multiple horizontal syncs per line and/or multiple vertical syncs per frame will be observed. These result in high peak throughput requirements, leading to DDR bandwidth being temporarily over-consumed, and thus VIP overflow.
The high level recovery method for VIP overflow on Port A is outlined in the steps below. Port B is similar.
1. Set VIP_XTRA6_PORT_A[31:16] YUV_SRCNUM_STOP_IMMEDIATELY = 0xFFFF_FFFF
2. Set VIP_XTRA6_PORT_A[15:0] ANC_SRCNUM_STOP_IMMEDIATELY = 0xFFFF_FFFF
3. Set VIP_PORT_A[8] ENABLE = 0
4. Set VIP_PORT_A[7] CLR_ASYNC_FIFO_RD and VIP_PORT_A[6] CLR_ASYNC_FIFO_WR to 1
5. Set VIP_PORT_A[23] SW_RESET to 1
6. Reset other VIP modules
7. Abort VPDMA channels
8. Set VIP_PORT_A[23] SW_RESET to 0
9. Un-reset other VIP modules
10. (Delay)
11. SC coeff downloaded (if VIP_SCALER is being used)
12. (Delay)
13. Set VIP_XTRA6_PORT_A[31:16] YUV_SRCNUM_STOP_IMMEDIATELY = 0x0000_0000
14. Set VIP_XTRA6_PORT_A[15:0] ANC_SRCNUM_STOP_IMMEDIATELY = 0x0000_0000
15. Set VIP_PORT_A[8] ENABLE = 1
16. Set VIP_PORT_A[7] CLR_ASYNC_FIFO_RD and VIP_PORT_A[6] CLR_ASYNC_FIFO_WR to 0