SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
This is the offset of the destination address from the initial destination address for the first access of the third loop. This will be added to the destination address from the loop before. This is a signed value so that the destination address can be both above and below the initial destination address.