SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
To support tracking of credits from each proxy thread, the proxy will extract the first word from the total message size for private tracking usage. This will include saving the proxy thread ID used within the proxy. This is necessary so that when a proxy reads a new message from the target it can inspect this word and return the credit to the source proxy thread. This allows the outbound proxy threads to have a set number of message credits, which decrement when a new message is written, and increment when a message from that proxy thread is read, thus keeping the credits in the system coherent. Any data written to this first word of the message will be ignored, so software should not write to the first word of messages through the proxy. Consumer software can use the first word to identify the source proxy thread of the message (SEC_PROXY_DATA_j).