SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
To enhance performance for DMAs, the RINGACC provides a bus that indicates when ring updates occur, allowing the DMA to track their own rings and detect updates before the responses arrive. The bus will go valid whenever there is an update to the state of a ring, which can be from a push, pop, or doorbell write. It will not go valid for a peek, a emudbg pop, a push to a full ring, as those do not update the ring state. When the bus is valid, the other signals are valid and indicate whether the operation was a push or a pop, whether the resulting state of the ring is empty, the ring number, and the number of elements updated to the ring (the push determines whether it is subtracted or added to the current count). One special case is a pop from an empty ring, which indicates an update but the element count is 0 since no items were actually popped, but a DMA using the cnt to add or subtract must handle this correctly by default. The bus will go valid once the operation command has been completed, and not after the response has been recevied, even for ring mode rings, allowing the DMA to see the update as soon as it is known by the RINGACC even before it is known to software.