SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
After the first N virtIDs for DMA class usage, the remaining virtIDs up to the maximum allowed (as set in PVU_VIRTID_MAP2) are for general usage. Each of these map one to one to a TLB, where the calculation is:
There are no classes used for this range of virtIDs. An input virtID that is beyond the MAX_CNT bitfield value will produce an error.