SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
The following firewalls are present in COMPUTE_CLUSTER0:
The A72SS0 firewall protects the traffic generated from the A72SS0 and is placed on the master port side unlike most device firewalls that are on the slave port side. This firewall has to be programed to enable the A72 master port access to the needed slaves.
The first C71SS0 region based firewall (C71SS0 MDMA) protects the traffic generated from the C71SS0 and same as A72SS0 is placed on the master port side. The second C71SS0 region based firewall protects the access to the C71SS0 L2 SRAM and is placed on the slave port side.
The DRU region based firewall is intended to protect the DRU configuration registers within a programmatically specified range. The DRU channelized firewall protects the following:
The A72SS0 and C71SS0 region based firewalls are same as the other device region based firewalls. For more information about their functionality, see Section 3.3.4 Interconnect Firewalls in Chapter 3 System Interconnect.