| Time-base (TB) | - Scale the time-base clock (TBCLK) relative to the system clock (FICLK).
- Configure the PWM time-base counter (TBCNT) frequency or period.
- Time-base counter mode selection:
- count-up mode: used for asymmetric PWM
- count-down mode: used for asymmetric PWM
- count-up-and-down mode: used for symmetric PWM
- Configure the time-base phase relative to another EPWM module.
- Synchronize the time-base counter between modules through hardware or software.
- Configure the direction (up or down) of the time-base counter after a synchronization event.
- Configure how the time-base counter will behave when the device is halted by an emulator.
- Specify the source for the synchronization output of the EPWM module:
- Synchronization input signal
- Time-base counter equal to zero
- Time-base counter equal to counter-compare B (CMPB)
- No output synchronization signal generated
|
| Counter-compare (CC) | - Specify the PWM duty cycle for output EPWMxA and/or output EPWMxB
- Specify the time at which switching events occur on the EPWMxA or EPWMxB output
|
| Action-qualifier (AQ) | - Specify the type of action taken when a time-base or counter-compare submodule event occurs:
- No action taken
- Output EPWMxA and/or EPWMxB switched high
- Output EPWMxA and/or EPWMxB switched low
- Output EPWMxA and/or EPWMxB toggled
- Force the PWM output state through software control
- Configure and control the PWM dead-band through software
|
| Dead-band (DB) | - Control of traditional complementary dead-band relationship between upper and lower switches
- Specify the output rising-edge-delay value
- Specify the output falling-edge delay value
- Bypass the dead-band module entirely. In this case the PWM waveform is passed through without modification
|
| PWM-chopper (PC) | - Create a chopping (carrier) frequency
- Pulse width of the first pulse in the chopped pulse train
- Duty cycle of the second and subsequent pulses
- Bypass the PWM-chopper module entirely. In this case the PWM waveform is passed through without modification.
|
| Trip-zone (TZ) | - Configure the EPWM module to react to one, all, or none of the trip-zone pins
- Specify the tripping action taken when a fault occurs:
- Force EPWMxA and/or EPWMxB high
- Force EPWMxA and/or EPWMxB low
- Force EPWMxA and/or EPWMxB to a high-impedance state
- Configure EPWMxA and/or EPWMxB to ignore any trip condition
- Configure how often the EPWM will react to the trip-zone pin:
- Enable the trip-zone to initiate an interrupt
- Bypass the trip-zone module entirely
|
Event-trigger (ET) | - Enable the EPWM events that will trigger an interrupt.
- Specify the rate at which events cause triggers (every occurrence or every second or third occurrence)
- Poll, set, or clear event flags
|
| High-Resolution PWM (HRPWM) | - Enable extended time resolution capabilities
- Configure finer time granularity control or edge positioning
|