The memory view of each R5F (that is, the memory map as seen by each R5F) is a function of several things:
- Exception vector bootstrap: The R5F exception table (including boot vector) is always 32 bytes at address 0x00000000 as seen by the R5F. If not booting from a TCM, then boot is done over the main memory interface. The exception vector bootstrap is under software control, which allows these 32 bytes at address 0x00000000 to be remapped somewhere else in the SoC memory map.
- TCM locations: TCMs can be enabled or disabled and located at different places in the memory map, depending on bootstrap configuration. For more details, see Table 6-26, and Section 6.3.3.2.2.
- Peripheral interface locatons: The RF5 natively supports three interfaces for peripheral access. Each can be enabled/disabled and located based on bootstrap configuration. Note that the VBUSP peripheral interface must be enabled in order to use RAT and VIM.
- RAT base address: This is determined by a bootstrap. This address is located within the VBUSP peripheral interface address space.
- VIM base address: This is determined by a bootstrap. This address is located within the VBUSP peripheral interface address space.
- RAT programming: The RAT can take regions of memory accessible by the main memory interface and map them to different addresses.
The combination of the above determines what the R5F sees where in the memory map, and over what interface different transactions come out. Every transaction that does not directly address a TCM or a peripheral interface comes over the main memory interface. Transactions on the main memory interface can be further remapped with the RAT.
See Chapter 2, Memory Map, for the complete R5F memory view for this device.