SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
Figure 3-10 VBUSM Block DiagramThe VBUSM Timeout Gasket tracks transactions outstanding on a VBUSM 4.0 initiator interface. If a transaction has been outstanding for more than a programmed time, the transaction is considered timed-out (with the expectation that the target is hung and will not return a response). The gasket will then signal an error to the system and provide responses (with appropriate error status) so that the initiator can proceed and will not be hung as well.