Peripheral firewall modules are placed in front of peripherals like UART, SPI and so forth. They protect access to the peripheral registers/memory and typically have firewall regions as number of regions supported by module that is being protected.
All Peripheral firewalls support 3 Priv-ID slots that allow multiple masters/initiators to access protected peripherals.
The peripheral firewall is configured using dedicated VBUSP port to CBASS that connects to DMSC private VBUSP interconnect.
Figure 3-4
presents Peripheral Firewall.
Each region is defined by start and end physical
address and associated permission/control register as shown in Figure 3-5.
A Peripheral's Firewall module can have one or more regions. In case there is more than 1 region, the registers are duplicated for each region.
If multiple regions are supported, a firewall configuration can be defined as either a Background or Foreground region depending on the setting of the Background (B) bit. Foreground regions can overlap background regions and their Firewall settings take precedence over the Background settings when there is overlap. However, background regions cannot overlap each other and foreground regions cannot overlap each other. A firewall error will result in case a memory transaction is made to the improper overlap regions.
Figure 3-6
presents peripherals firewall regions.
In the above case, Region 0 and Region 2 are background regions (background bit set in control register). Region 1, Region 3 and Region 4 are not background (foreground) regions. In case the incoming transaction hits in address in Region 1, the permissions of Region 1 are applied to filter incoming transaction, thereby completely ignoring the permission of the background Region 0.
Table 3-40 through Table 3-54 show the initiator and target firewalls, firewall IDs, physical base address of the
corresponding firewall, number of firewall regions, and areas covered by the firewall. The
firewall ID uniquely identifies each firewall. In case of firewall violation this ID is
logged and can be read through the CBASS_EXCEPTION_LOGGING_HEADER0[23-8] SRC_ID field.
Table 3-40 CBASS_AASRC0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| AASRC0_CFG |
2608 |
1 |
0x4528C000 |
| AASRC0_DATA |
2609 |
2 |
0x4528C400 |
| CBASS_AASRC0_ERR |
2623 |
1 |
0x4528FC00 |
Table 3-41 CBASS_AC0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| There are no slave ports of modules or
subsystems on this sub-interconnect |
N/A |
N/A |
N/A |
Table 3-42 CBASS_CSI0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| CSI_RX0 |
2432 |
4 |
0x45260000 |
| CSI_RX1 |
2433 |
4 |
0x45260400 |
| DPHY_RX0 |
2436 |
2 |
0x45261000 |
| DPHY_RX1 |
2437 |
2 |
0x45261400 |
| CSI_TX0 |
2440 |
4 |
0x45262000 |
| DPHY_TX0 |
2442 |
1 |
0x45262800 |
| CSI_PSIL0_CFG |
2446 |
1 |
0x45263800 |
| CBASS_CSI0_ERR |
2463 |
1 |
0x45267C00 |
Table 3-43 CBASS_DATADEBUG0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| STM0 |
2464 |
2 |
0x45268000 |
| DEBUGSS0_CFG |
2465 |
1 |
0x45268400 |
| MAIN_DEBUG_CELL0 |
2466 |
1 |
0x45268800 |
| CC_DEBUG_CELL0 |
2467 |
1 |
0x45268C00 |
| MAIN_DEBUG_CELL1 |
2468 |
1 |
0x45269000 |
| C66SS0_DEBUG_CELL |
2469 |
1 |
0x45269400 |
| C66SS1_DEBUG_CELL |
2470 |
1 |
0x45269800 |
| PDMA_DEBUG_PSIL0_CFG |
2472 |
1 |
0x4526A000 |
| CBASS_DATADEBUG0_ERR |
2495 |
1 |
0x4526FC00 |
Table 3-44 CBASS_HC_CFG0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| PCIE0_CFG |
2560 |
8 |
0x45280000 |
| PCIE1_CFG |
2561 |
8 |
0x45280400 |
| PCIE2_CFG |
2562 |
8 |
0x45280800 |
| PCIE3_CFG |
2563 |
8 |
0x45280C00 |
| USB3SS0_CORE |
2568 |
4 |
0x45282000 |
| USB3SS0_USB2PHY |
2569 |
1 |
0x45282400 |
| USB3SS1_CORE |
2570 |
4 |
0x45282800 |
| USB3SS1_USB2PHY |
2571 |
1 |
0x45282C00 |
| MMCSD0_CFG |
2576 |
4 |
0x45284000 |
| MLBSS0_CFG |
2578 |
4 |
0x45284800 |
| UFS0_CFG |
2580 |
4 |
0x45285000 |
| HC5_ECC_AGGR_CFG |
2583 |
1 |
0x45285C00 |
| SERDES0 |
2584 |
1 |
0x45286000 |
| SERDES1 |
2585 |
1 |
0x45286400 |
| SERDES2 |
2586 |
1 |
0x45286800 |
| SERDES3 |
2587 |
1 |
0x45286C00 |
| PBIST_HC0_CFG |
2588 |
1 |
0x45287000 |
| CBASS_HC2_0_ERR |
2589 |
1 |
0x45287400 |
| CBASS_HC0_ERR |
2590 |
1 |
0x45287800 |
| CBASS_HC_CFG0_ERR |
2591 |
1 |
0x45287C00 |
Table 3-45 CBASS_HC0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| PCIE0_HP |
2528 |
24 |
0x45278000 |
| PCIE0_LP |
2529 |
24 |
0x45278400 |
| PCIE1_HP |
2530 |
24 |
0x45278800 |
| PCIE1_LP |
2531 |
24 |
0x45278C00 |
| PCIE2_HP |
2532 |
24 |
0x45279000 |
| PCIE2_LP |
2533 |
24 |
0x45279400 |
| PCIE3_HP |
2534 |
24 |
0x45279800 |
| PCIE3_LP |
2535 |
24 |
0x45279C00 |
Table 3-46 CBASS_HC2_0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| There are no slave ports of modules or
subsystems on this sub-interconnect |
N/A |
N/A |
N/A |
Table 3-47 CBASS_IPPHY0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| EPWM0 |
2048 |
1 |
0x45200000 |
| HRPWM0 |
2049 |
1 |
0x45200400 |
| EPWM1 |
2050 |
1 |
0x45200800 |
| HRPWM1 |
2051 |
1 |
0x45200C00 |
| EPWM2 |
2052 |
1 |
0x45201000 |
| HRPWM2 |
2053 |
1 |
0x45201400 |
| EPWM3 |
2054 |
1 |
0x45201800 |
| HRPWM3 |
2055 |
1 |
0x45201C00 |
| EPWM4 |
2056 |
1 |
0x45202000 |
| HRPWM4 |
2057 |
1 |
0x45202400 |
| EPWM5 |
2058 |
1 |
0x45202800 |
| HRPWM5 |
2059 |
1 |
0x45202C00 |
| EQEP0 |
2064 |
1 |
0x45204000 |
| EQEP1 |
2065 |
1 |
0x45204400 |
| EQEP2 |
2066 |
1 |
0x45204800 |
| ECAP0 |
2068 |
1 |
0x45205000 |
| ECAP1 |
2069 |
1 |
0x45205400 |
| ECAP2 |
2070 |
1 |
0x45205800 |
| I2C0 |
2072 |
1 |
0x45206000 |
| I2C1 |
2073 |
1 |
0x45206400 |
| I2C2 |
2074 |
1 |
0x45206800 |
| I2C3 |
2075 |
1 |
0x45206C00 |
| I2C4 |
2076 |
1 |
0x45207000 |
| I2C5 |
2077 |
1 |
0x45207400 |
| I2C6 |
2078 |
1 |
0x45207800 |
| ATL0 |
2080 |
1 |
0x45208000 |
| I3C0 |
2082 |
4 |
0x45208800 |
| RTI0 |
2086 |
1 |
0x45209800 |
| RTI1 |
2087 |
1 |
0x45209C00 |
| RTI28 |
2094 |
1 |
0x4520B800 |
| RTI29 |
2095 |
1 |
0x4520BC00 |
| RTI30 |
2096 |
1 |
0x4520C000 |
| RTI31 |
2097 |
1 |
0x4520C400 |
| RTI16 |
2100 |
1 |
0x4520D000 |
| RTI24 |
2104 |
1 |
0x4520E000 |
| RTI25 |
2105 |
1 |
0x4520E400 |
| RTI15 |
2108 |
1 |
0x4520F000 |
| TIMER0 |
2112 |
1 |
0x45210000 |
| TIMER1 |
2113 |
1 |
0x45210400 |
| TIMER2 |
2114 |
1 |
0x45210800 |
| TIMER3 |
2115 |
1 |
0x45210C00 |
| TIMER4 |
2116 |
1 |
0x45211000 |
| TIMER5 |
2117 |
1 |
0x45211400 |
| TIMER6 |
2118 |
1 |
0x45211800 |
| TIMER7 |
2119 |
1 |
0x45211C00 |
| TIMER8 |
2120 |
1 |
0x45212000 |
| TIMER9 |
2121 |
1 |
0x45212400 |
| TIMER10 |
2122 |
1 |
0x45212800 |
| TIMER11 |
2123 |
1 |
0x45212C00 |
| TIMER12 |
2124 |
1 |
0x45213000 |
| TIMER13 |
2125 |
1 |
0x45213400 |
| TIMER14 |
2126 |
1 |
0x45213800 |
| TIMER15 |
2127 |
1 |
0x45213C00 |
| TIMER16 |
2128 |
1 |
0x45214000 |
| TIMER17 |
2129 |
1 |
0x45214400 |
| TIMER18 |
2130 |
1 |
0x45214800 |
| TIMER19 |
2131 |
1 |
0x45214C00 |
| SPI0 |
2136 |
1 |
0x45216000 |
| SPI1 |
2137 |
1 |
0x45216400 |
| SPI2 |
2138 |
1 |
0x45216800 |
| SPI3 |
2139 |
1 |
0x45216C00 |
| SPI4 |
2140 |
1 |
0x45217000 |
| SPI5 |
2141 |
1 |
0x45217400 |
| SPI6 |
2142 |
1 |
0x45217800 |
| SPI7 |
2143 |
1 |
0x45217C00 |
| UART0 |
2148 |
1 |
0x45219000 |
| UART1 |
2149 |
1 |
0x45219400 |
| UART2 |
2150 |
1 |
0x45219800 |
| UART3 |
2151 |
1 |
0x45219C00 |
| UART4 |
2152 |
1 |
0x4521A000 |
| UART5 |
2153 |
1 |
0x4521A400 |
| UART6 |
2154 |
1 |
0x4521A800 |
| UART7 |
2155 |
1 |
0x4521AC00 |
| UART8 |
2156 |
1 |
0x4521B000 |
| UART9 |
2157 |
1 |
0x4521B400 |
| MCAN0 |
2160 |
4 |
0x4521C000 |
| MCAN1 |
2161 |
4 |
0x4521C400 |
| MCAN2 |
2162 |
4 |
0x4521C800 |
| MCAN3 |
2163 |
4 |
0x4521CC00 |
| MCAN4 |
2164 |
4 |
0x4521D000 |
| MCAN5 |
2165 |
4 |
0x4521D400 |
| MCAN6 |
2166 |
4 |
0x4521D800 |
| MCAN7 |
2167 |
4 |
0x4521DC00 |
| MCAN8 |
2168 |
4 |
0x4521E000 |
| MCAN9 |
2169 |
4 |
0x4521E400 |
| MCAN10 |
2170 |
4 |
0x4521E800 |
| MCAN11 |
2171 |
4 |
0x4521EC00 |
| MCAN12 |
2172 |
4 |
0x4521F000 |
| MCAN13 |
2173 |
4 |
0x4521F400 |
| PDMA_MISC_PSIL0_CFG |
2184 |
1 |
0x45222000 |
| PDMA_USART_PSIL0_CFG |
2185 |
1 |
0x45222400 |
| CBASS_IPPHY0_ERR |
2303 |
1 |
0x4523FC00 |
Table 3-48 CBASS_MCASP_G0_0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| MCASP0_CFG |
2592 |
1 |
0x45288000 |
| MCASP0_DMA |
2593 |
1 |
0x45288400 |
| MCASP1_CFG |
2594 |
1 |
0x45288800 |
| MCASP1_DMA |
2595 |
1 |
0x45288C00 |
| MCASP2_CFG |
2596 |
1 |
0x45289000 |
| MCASP2_DMA |
2597 |
1 |
0x45289400 |
| PDMA_AASRC_PSIL0_CFG |
2606 |
1 |
0x4528B800 |
| CBASS_MCASP_G0_0_ERR |
2607 |
1 |
0x4528BC00 |
Table 3-49 CBASS_MCASP_G1_0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| MCASP3_CFG |
2496 |
1 |
0x45270000 |
| MCASP3_DMA |
2497 |
1 |
0x45270400 |
| MCASP4_CFG |
2498 |
1 |
0x45270800 |
| MCASP4_DMA |
2499 |
1 |
0x45270C00 |
| MCASP5_CFG |
2500 |
1 |
0x45271000 |
| MCASP5_DMA |
2501 |
1 |
0x45271400 |
| MCASP6_CFG |
2502 |
1 |
0x45271800 |
| MCASP6_DMA |
2503 |
1 |
0x45271C00 |
| MCASP7_CFG |
2504 |
1 |
0x45272000 |
| MCASP7_DMA |
2505 |
1 |
0x45272400 |
| MCASP8_CFG |
2506 |
1 |
0x45272800 |
| MCASP8_DMA |
2507 |
1 |
0x45272C00 |
| MCASP9_CFG |
2508 |
1 |
0x45273000 |
| MCASP9_DMA |
2509 |
1 |
0x45273400 |
| MCASP10_CFG |
2510 |
1 |
0x45273800 |
| MCASP10_DMA |
2511 |
1 |
0x45273C00 |
| MCASP11_CFG |
2512 |
1 |
0x45274000 |
| MCASP11_DMA |
2513 |
1 |
0x45274400 |
| CBASS_MCASP_G1_0_ERR |
2527 |
1 |
0x45277C00 |
Table 3-50 CBASS_RC_CFG0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| R5FSS0_CORE0_CFG |
2368 |
2 |
0x45250000 |
| R5FSS0_CORE1_CFG |
2369 |
1 |
0x45250400 |
| R5FSS1_CORE0_CFG |
2370 |
2 |
0x45250800 |
| R5FSS1_CORE1_CFG |
2371 |
1 |
0x45250C00 |
| C66SS0_CFG |
2376 |
1 |
0x45252000 |
| C66SS1_CFG |
2377 |
1 |
0x45252400 |
| MMCSD1_CFG |
2380 |
4 |
0x45253000 |
| MMCSD2_CFG |
2381 |
4 |
0x45253400 |
| ELM0 |
2384 |
1 |
0x45254000 |
| PRU_ICSSG0 |
2386 |
8 |
0x45254800 |
| PRU_ICSSG1 |
2387 |
8 |
0x45254C00 |
| CPSW0 |
2390 |
2 |
0x45255800 |
| VPFE0_RATCFG |
2394 |
1 |
0x45256800 |
| VPFE0_CFG |
2395 |
1 |
0x45256C00 |
| NAVSS0_NBSS_CFG |
2398 |
7 |
0x45257800 |
| COMPUTE_CLUSTER0 |
2400 |
16 |
0x45258000 |
| RCNAVSS11_ECC_AGGR_CFG |
2408 |
1 |
0x4525A000 |
| RC4_ECC_AGGR_CFG |
2409 |
1 |
0x4525A400 |
| RC_R500_ECC_AGGR_CFG |
2410 |
1 |
0x4525A800 |
| RC_R511_ECC_AGGR_CFG |
2411 |
1 |
0x4525AC00 |
| RCNAVSS10_ECC_AGGR_CFG |
2415 |
1 |
0x4525BC00 |
| PBIST_RC_NAVSS_CFG |
2416 |
1 |
0x4525C000 |
| PBIST_RC_NB_CFG |
2417 |
1 |
0x4525C400 |
| PBIST_RC_R5FSS0_CFG |
2418 |
1 |
0x4525C800 |
| PBIST_RC_R5FSS1_CFG |
2419 |
1 |
0x4525CC00 |
| CBASS_RC0_ERR |
2430 |
1 |
0x4525F800 |
| CBASS_RC_CFG0_ERR |
2431 |
1 |
0x4525FC00 |
Table 3-51 CBASS_RC0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| C66SS0_SRC |
2304 |
8 |
0x45240000 |
| C66SS1_SRC |
2305 |
8 |
0x45240400 |
| GPMC0 |
2310 |
8 |
0x45241800 |
| R5FSS0_CORE0 |
2314 |
4 |
0x45242800 |
| R5FSS0_CORE1 |
2315 |
4 |
0x45242C00 |
| R5FSS1_CORE0 |
2316 |
4 |
0x45243000 |
| R5FSS1_CORE1 |
2317 |
4 |
0x45243400 |
Table 3-52 INFRA_CBASS0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| PSRAM2KECC0 |
1 |
1 |
0x45000400 |
| PSRAM2KECC0_ECCAGGR |
2 |
1 |
0x45000800 |
| PSC0 |
5 |
1 |
0x45001400 |
| PLLCTRL0 |
6 |
1 |
0x45001800 |
| GTC0 |
7 |
4 |
0x45001C00 |
| PLL0_CFG |
8 |
26 |
0x45002000 |
| CTRL_MMR0 |
9 |
16 |
0x45002400 |
| EFUSE0 |
11 |
1 |
0x45002C00 |
| PBIST_INFRA0_CFG |
12 |
1 |
0x45003000 |
| GPIO0 |
16 |
1 |
0x45004000 |
| GPIO1 |
17 |
1 |
0x45004400 |
| GPIO2 |
18 |
1 |
0x45004800 |
| GPIO3 |
19 |
1 |
0x45004C00 |
| GPIO4 |
20 |
1 |
0x45005000 |
| GPIO5 |
21 |
1 |
0x45005400 |
| GPIO6 |
22 |
1 |
0x45005800 |
| GPIO7 |
23 |
1 |
0x45005C00 |
| ESM0_CFG |
24 |
1 |
0x45006000 |
| DCC0 |
32 |
1 |
0x45008000 |
| DCC1 |
33 |
1 |
0x45008400 |
| DCC2 |
34 |
1 |
0x45008800 |
| DCC3 |
35 |
1 |
0x45008C00 |
| DCC4 |
36 |
1 |
0x45009000 |
| DCC5 |
37 |
1 |
0x45009400 |
| DCC6 |
38 |
1 |
0x45009800 |
| DCC7 |
39 |
1 |
0x45009C00 |
| DCC8 |
40 |
1 |
0x4500A000 |
| DCC9 |
41 |
1 |
0x4500A400 |
| DCC10 |
42 |
1 |
0x4500A800 |
| DCC11 |
43 |
1 |
0x4500AC00 |
| DCC12 |
44 |
1 |
0x4500B000 |
| GPIOMUX_INTRTR0_CFG |
56 |
1 |
0x4500E000 |
| MAIN2MCU_LVL_INTRTR0_CFG |
57 |
1 |
0x4500E400 |
| MAIN2MCU_PLS_INTRTR0_CFG |
58 |
1 |
0x4500E800 |
| CMPEVT_INTRTR0_CFG |
59 |
1 |
0x4500EC00 |
| TIMESYNC_INTRTR0_CFG |
60 |
1 |
0x4500F000 |
| MAIN_MCU1_INTROUTER0 |
62 |
1 |
0x4500F800 |
| MAIN_MCU0_INTROUTER0 |
63 |
1 |
0x4500FC00 |
| C66SS0_INTRTR0_CFG |
64 |
1 |
0x45010000 |
| C66SS0_INTRTR0_CFG |
65 |
1 |
0x45010400 |
| FW_CBASS0_ERR |
73 |
1 |
0x45012400 |
| INFRA_CBASS0_ERR |
74 |
1 |
0x45012800 |
| INFRA_ECC_AGGR0_CFG |
81 |
1 |
0x45014400 |
| PSRAMECC0 |
84 |
1 |
0x45015000 |
| PSRAMECC0_ECCAGGR |
85 |
1 |
0x45015400 |
Table 3-53 MCU_CBASS0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| MCU_R5FSS0_CORE0 |
1024 |
4 |
0x45100000 |
| MCU_R5FSS0_CORE0_CFG |
1025 |
2 |
0x45100400 |
| MCU_RTI0 |
1026 |
1 |
0x45100800 |
| MCU_R5FSS0_CORE1 |
1028 |
4 |
0x45101000 |
| MCU_R5FSS0_CORE1_CFG |
1029 |
1 |
0x45101400 |
| MCU_RTI1 |
1030 |
1 |
0x45101800 |
| MCU_FSS0_CFG |
1032 |
12 |
0x45102000 |
| MCU_FSS0_S1 |
1033 |
8 |
0x45102400 |
| MCU_FSS0_S0 |
1036 |
8 |
0x45103000 |
| MCU_PSROM0 |
1048 |
1 |
0x45106000 |
| MCU_MSRAM_1MB0 |
1050 |
8 |
0x45106800 |
| MCU_MSRAM_1MB0_CFG |
1051 |
1 |
0x45106C00 |
| MCU_PSRAM0 |
1052 |
1 |
0x45107000 |
| MCU_TIMER0 |
1056 |
1 |
0x45108000 |
| MCU_TIMER1 |
1057 |
1 |
0x45108400 |
| MCU_TIMER2 |
1058 |
1 |
0x45108800 |
| MCU_TIMER3 |
1059 |
1 |
0x45108C00 |
| MCU_TIMER4 |
1060 |
1 |
0x45109000 |
| MCU_TIMER5 |
1061 |
1 |
0x45109400 |
| MCU_TIMER6 |
1062 |
1 |
0x45109800 |
| MCU_TIMER7 |
1063 |
1 |
0x45109C00 |
| MCU_TIMER8 |
1064 |
1 |
0x4510A000 |
| MCU_TIMER9 |
1065 |
1 |
0x4510A400 |
| MCU_SPI0 |
1072 |
1 |
0x4510C000 |
| MCU_SPI1 |
1073 |
1 |
0x4510C400 |
| MCU_SPI2 |
1074 |
1 |
0x4510C800 |
| MCU_DCC0 |
1088 |
1 |
0x45110000 |
| MCU_DCC1 |
1089 |
1 |
0x45110400 |
| MCU_DCC2 |
1090 |
1 |
0x45110800 |
| MCU_ADC0_DMA |
1104 |
1 |
0x45114000 |
| MCU_ADC0_CFG |
1105 |
2 |
0x45114400 |
| MCU_ADC1_DMA |
1106 |
1 |
0x45114800 |
| MCU_ADC1_CFG |
1107 |
2 |
0x45114C00 |
| MCU_UART0 |
1120 |
1 |
0x45118000 |
| MCU_I2C0 |
1152 |
1 |
0x45120000 |
| MCU_I2C1 |
1153 |
1 |
0x45120400 |
| MCU_I3C0 |
1160 |
4 |
0x45122000 |
| MCU_I3C1 |
1161 |
4 |
0x45122400 |
| MCU_ESM0_CFG |
1168 |
1 |
0x45124000 |
| MCU_MCAN0 |
1184 |
4 |
0x45128000 |
| MCU_MCAN1 |
1185 |
4 |
0x45128400 |
| MCU_CTRL_MMR0 |
1200 |
8 |
0x4512C000 |
| MCU_PLL0_CFG |
1201 |
3 |
0x4512C400 |
| MCU_EFUSE0 |
1208 |
1 |
0x4512E000 |
| MCU_PBIST0_CFG |
1212 |
1 |
0x4512F000 |
| MCU_PBIST_R5FSS0_CFG |
1213 |
1 |
0x4512F400 |
| MCU_CPSW0 |
1220 |
2 |
0x45131000 |
| MCU_CBASS0_ERR |
1244 |
1 |
0x45137000 |
| MCU_FW_CBASS0_ERR |
1246 |
1 |
0x45137800 |
| MCU_ECC_AGGR0_CFG |
1253 |
1 |
0x45139400 |
Table 3-54 WKUP_CBASS0 Slave Modules Attributes
| Slaves |
Firewall ID |
Firewall Regions |
Firewall Physical Address |
| WKUP_PSC0 |
129 |
1 |
0x45020400 |
| WKUP_PLLCTRL0 |
130 |
1 |
0x45020800 |
| WKUP_CTRL_MMR0 |
131 |
16 |
0x45020C00 |
| WKUP_GPIO0 |
132 |
1 |
0x45021000 |
| WKUP_ESM0_CFG |
133 |
1 |
0x45021400 |
| WKUP_VTM0 |
135 |
3 |
0x45021C00 |
| WKUP_GPIO1 |
137 |
1 |
0x45022400 |
| WKUP_I2C0 |
144 |
1 |
0x45024000 |
| WKUP_UART0 |
160 |
1 |
0x45028000 |
| WKUP_GPIOMUX_INTRTR0_CFG |
168 |
1 |
0x4502A000 |
| WKUP_CBASS0_ERR |
176 |
1 |
0x4502C000 |
| WKUP_FW_CBASS0_ERR |
177 |
1 |
0x4502C400 |
| WKUP_ECC_AGGR0_CFG |
178 |
1 |
0x4502C800 |