SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
The static field is used to allow for a single TR to be reused repeatedly. If the static bit is set then the UTC upon completing the specified TR will restart the TR with the same values as were in the initial TR. This TR will stay active until the channel is torn down. The initiating of a tear down of the channel will clear the STATIC field in the active TR and it will be removed from the channel FIFO after the TR completion.
If a TR is submitted to a channel FIFO with the STATIC field set then any TRs placed in the FIFO after that will NOT be run until the teardown has been initiated.