SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
| Parameter | Value |
|---|---|
| num_writes |
This is the number of outstanding write transactions that the write scoreboard can handle at once. When the scoreboard is full, all subsequent commands will be stalled, so this value should be picked appropriately for throughput. See Section 3.3.5.2.1.6.
|
| num_reads |
This is the number of outstanding read transactions that the read scoreboard can handle at once. When the scoreboard is full, all subsequent commands will be stalled, so this value should be picked appropriately for throughput. See Section 3.3.5.2.1.7.
|
| safe |
Add CBA Safety Signaling on the config bus and internal flop protection. Include EDC controller and export sVbus interface(s)
|
| safe_bus |
Add CBA Safety Signaling on the source and destination VBUSM interfaces
|
| src_name | This is the prefix for the signals on the source bus |
| dst_name | This is the prefix for the signals on the destination bus |
| osigs | Space separate list of optional signals on the CBA interfaces |
| data_wdth | Width of the data bus. Default 32 |
| addr_wdth | Width of the address bus. Default 32 |
| region_cnt | Number of CBA Regions. Default 1 |
| pipe | Enable EDC Pipe Stage. Default 0 (off) |