SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
The final stage of the raw data mode is the line output control, which controls how the input sensor lines are written to external memory. The value of the bits in the VPFE_SDR_ADDR register defines the starting address where the frame should be written in external memory. The value of the VPFE_HSIZE_OFF[15-0] LNOFST bitfield defines the distance between the beginning of output lines in bytes. Both the starting address and line offset must be aligned to 32-byte boundaries (that is, either 16 or 32 pixels, depending on the VPFE_SYNMODE[11] PACK8 bit). Use the VPFE_SDOFST register to define additional offsets, depending on the field ID and the even/odd line numbers.
Figure 12-1194 shows example of input and output images in the two formats - non-inversed and inversed.