SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
There needs to be at least a ping-pong (2 deep) buffer in SL2 for the disparity output. The size of the output can vary based on the location of the processed block in the frame. The height of the block will have one particular value for the first row of blocks in the image. Then, in steady state, the height would have a different value for the central part of the image rows. It would finally have a different height for the last row of blocks. The UTC needs to be configured appropriately to handle this. One possible way is to use 3 linked TR entries in UTC for these three image regions. The UTC needs to send out a block on every event trigger. Every block of this buffer will start from a new SL2 word.